REGEN.WATTEXT

Description

Sets the regen resistor's power fault level for an external regen resistor (when REGEN.TYPE = -1).

Above this fault level, the regen resistor's PWM will be 0 and a fault will be issued.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

W

Range

0 to (2500W for MV and 5000W for HV)

Default Value

1000 W

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.WATTEXT

3007h

04h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.WATTEXT

2404

964

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.WATTEXT

2404

Unsigned16

Read/Write

-